One cell specific reference signal is transmitted from each downlink antenna port.
The downlink cell specific reference signal can be used for the following purposes:
Cell search and initial acquisition
Downlink channel quality measurements
Downlink channel estimation for coherent demodulation/detection at the UE
Additional Downlink parameters are described in Cell Parameters (Basic LTE FDD Downlink), Synchronization Signals (Basic LTE FDD Downlink), and Power Relevant Parameters (Basic LTE FDD Downlink).
Range: -60 to 20 dB
Default: 0.000 dB
Enter a power level in dB for the cell specific reference signal.